Retail Reference Guide

The Retail Reference Guide is designed to give an overview of the Low Voltage products sold in retail environments. Click here for more information.


Content of the Guide

  • Arc fault circuit interrupters (AFCI) use advanced electronic technology to provide maximum available protection against the effects of arcing faults.

  • Ground fault circuit interrupter (GFCI) is designed to protect against severe electrical shock or electrocution from ground faults. Ground faults occur when the electrical current in an appliance strays outside its normal path, and the human body becomes part of the path through which the electrical current may flow.

  • PL and ES Series Loadcenters - A load center is the point where all of the electricity enters and is distributed throughout the house.

  • QN and MPD Breakers - The QN is used as both a branch breaker and a main breaker in applications which require a two pole,120/240V AC breaker.

  • MBK Breakers - Main breaker used in various Siemens load centers

  • QP Breakers - 1” pole center branch breaker

  • QT Breakers - 1/2” pole centers branch breakers offered as a duplex,triplex, and quadplex.

  • Surge Protection Device - 2” Wide plug-on containing two one pole circuit breakers and a surge arrester.


Did this information help you?