The Intelli-Arc Diagnostic Tool makes it easier to troubleshoot AFCI circuits by improving troubleshooting accuracy and reducing the number of visits to the problem site. The diagnostic tool can be used with any circuit breaker, regardless of brand.
Arc faults are often intermittent which can make troubleshooting the branch circuit very difficult. In these cases, it is important to determine whether the fault condition exists in the permanent wiring, in connected equipment, or in a power cord.
The Siemens Intelli-Arc Diagnostic Tool helps to accurately diagnose the circuit in which a fault has occurred. When used in conjunction with good troubleshooting techniques, this tool allows the electrical contractor to determine and locate the root cause or source of the fault. The device presents information as to the type and magnitude of fault. Since the fault may not cause an AFCI to trip for various reasons, i.e. duration too short, current level too low, the tool provides an indication showing how close an event is to causing an AFCI to trip.
Improves troubleshooting accuracy
Reduce time spent and number of trips to problem site
Simplistic setup: wire in, wire out to use
Wireless communication – enables “1 person” troubleshooting
Can be used to troubleshoot any AFCI circuit, regardless of brand
LED Indicators: provides status level for current, ground fault, and arc fault
Status indicators: provides confirmation of power and communication connection