Building Technologies and Solutions

Facility Mobile Applications: Facility Prime & Facility to Go

Facility Prime Wins CSE 2013 "Product of the Year" Gold Award

Siemens Wins CSE 2013 Product of the Year Gold Award

Congratulations to the entire Facility Prime Mobile Application Team! The Facility Prime Mobile Application, was chosen as one of the best new products of 2013 by the readers of Consulting-Specifying Engineer. The Facility Prime Mobile Application took the Gold award in the Networked BAS, energy management systems category in Consulting-Specifying Engineer’s 2013 Product of the Year program.

Consulting-Specifying Engineer's Product of the Year program is the premier award for new products in the HVAC, fire/life safety, electrical, and plumbing systems engineering markets. As a winner of Consulting Specifying Engineer’s Product of the Year contest, the Facility Prime Mobile Application was highlighted in the September 2013 issue of Consulting-Specifying Engineer.

Facility to Go

Facility to Go

Facility to Go is a text-based smart phone app used for point monitoring and commanding.  This app utilizes BACnet Web Server to connect directly to a Siemens field panel and allows the user complete access to all points on the panel.  No customization required.  Must have a web services license enabled.

Available at the Android Market

Available at the Blackberry World


Facility Prime

Facility Prime

The Facility PrimeTM application is a building management iPad® application for interaction with the APOGEE Building Automation System (BAS). Through customized screens, Facility Prime enables quick, mobile interaction to view only or view and command environmental conditions and HVAC control systems. Facility Prime goes beyond accessing data and provides two-way interaction between users and the building automation system. Users develop customized graphics for their facility using Facility Prime Editor or contracting their local Siemens office to create the graphics.

Facility Prime Available on App Store


Facility Prime Editor

Facility Prime Editor

The Facility PrimeTM Editor application provides all the capabilities of the Facility Prime application as well as the ability to create and modify the graphics to exact user needs. Proper log-on and password authentication with a Siemens APOGEE IP panel is required to enable Facility Prime Editor’s configuration functions. A library of graphical elements containing gauges, graphs, device images and position animation is included with Facility Prime Editor. In addition, editors may import documents, photos, and images to be used in their graphics. Building automation controller data and equipment settings are linked to graphics by entering point address information. Significant knowledge of the BAS is required for configuration of the screens and point data.

Facility Prime Editor Available on App Store

Did this information help you?